Other Parts Discussed in Thread: CC2541
Hi,
I would like to build my application on CC2541 and if I choose to develop my application on the CC2541EM boards, I will also need to buy the CC2540DK,
which comes with 2 of SmartRF05EB, which is the baseboard onto which the CC2541EM (daughter) boards sit
I read that I will need "SOC-BB board" for stand alone operation of each CC2541EM board. The SOC-BB board has 2xAA battery holders that power the CC2541EM board sitting on it. Please see link below:
http://media.digikey.com/Photos/Texas%20Instr%20Photos/SOC-BB.jpg
According to the photo above, there is also a debug port on the SOC-BB boards that can be used for debugging and flashing code on to the CC2541EM board. Is this correct? If that is the case, I do not need to buy the expensive CC2540DK product to do my code development and debugging. Is this correct?
Do I need any other hardware to get the CC2541EM boards to work stand alone?
Also, all that applies to CC2541EM boards also applies to the CC2540EM boards I presume. Can you please comment?
I appreciate your kind support.
Regards...