Other Parts Discussed in Thread: CC2540
Hi,
I have used the CC2540 mini EMK for a project with the iphone.
Everything was working all right.
Now i bought some extra modules to expaned the BLE are but the program on the iphone is getting stuck when i use the new modules.
I copied the hex file from the old module to the new CC2540 module. It works with the old CC2540 module (bought last year) but with the one bought this month the program crashes.
Is there made a change to the board of the CC2540 or do i need an newer ioCC2540.h file ?
The "old" version is 1.5.1 / CC2540DK_EM.
On the newest the version is CC2540DK_EM / 1.5.1.1
Kind regards,
Davy