This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issue with CC2540DK leds on SmartRF05 board

Hello

I need to blink a led on the SmartRF05 board when i receive a packet (no matter the details, i will use it as a signal for time measurements) in the SimpleBLEPeripheral demo project. 

I opened the project in IAR and inserted the HalLedSet instructions. Nothing Happened, so i used HalLedSet( HAL_LED_ALL, HAL_LED_MODE_OFF ) for test, but leds are still all turned on (exept for led4) . I tried to move the instruction at different points of the program flow, but the result is still the same.

It seems i have not control over them! Could anyone help me please?