This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About TI CC2540 DK

Dear engineers of TI,

I want to build a demo. In this demo, there are three nodes. Each node contains a RF smart 05EB+BLE module. What I want is to use one node to make other two nodes connect with each other. Can it feasible?    

I build it because I want to use this demo to solve a problem in real world. In this demo, one node represents a lamp,  one node represents a smartphone and one node represents a router(which supports BLE technology). The scenario is that a user has brought a BLE lamp. He also has a smartphone. He can use this smartphone to control this lamp through BLE technology. However, when he wants to leave, the lamp can not be controlled. So he thinks about a solution to this problem. Because there is a router which supports BLE technology in his house. His idea is that he makes the lamp connect with the router when he is not in the house. In addtion, by using this solution, he can remote control the lamp via Internet. The question is that the lamp and the router both do not have buttons, they can not connect with each other by themselves. So I want to use the smartphone to make the lamp and the router connect. In this small demo, the problem is to use one node to make the other two nodes connect. 

Best Regards