This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GAP_DEVICE_INFO_EVENT missing on the masterSlaveSwitch app for CC2541DK-MINI Keyfob using v1.2

Other Parts Discussed in Thread: CC2541, CC2541DK-MINI

Hi

I'm using the the masterSlaveSwitch app as the basis of a project I'm working on for the CC2541DK-MINI Keyfob using v1.2 ie linking against CC2541_ble_single_chip_all. The problem I'm having is seeing the GAP_DEVICE_INFO_EVENT my callback looks like this:

static void blePlatformCentralEventCB(gapCentralRoleEvent_t *pEvent)
{
  switch (pEvent->gap.opcode)
  {
  case GAP_DEVICE_INIT_DONE_EVENT:
    GAPCentralRole_StartDiscovery(DEFAULT_DISCOVERY_MODE, DEFAULT_DISCOVERY_ACTIVE_SCAN, DEFAULT_DISCOVERY_WHITE_LIST);
    break;
    
  ....

  case GAP_DEVICE_DISCOVERY_EVENT:
  case GAP_DEVICE_INFO_EVENT:
    seeWhatIsAdvert();

It never hits the seeWhatIsAdvert even though I can verify there are ads from an app (simpleBLEPeripheral) and I can discover this device using the BTool commands.

Are there any gotcha's in setup I'm using?

TIA

Kevin