Hi,
I have a couple of different custom hardware designs using CC2540, which I would like to be able to update using UBL.
I am able to update using an unmodified UBL from BLE-CC254x-1_3_2 and a software made from the HostTestApp example. To be able to run the UBL at startup I have to pull P1.2 low, but because of the different hardware designs I need to use another pin.
I have read "Universal Boot Loader for SOC-8051 by USB-MSD Developer’s Guide" and from that I understand that the pin is defined in the *.CFG file - isn't that right?
My question is how do I change the pin? I cannot read the default *.CFG and to me it seams like a big task to create a new config file from scratch. Do you have a tool that can help me generate the file?
Thanks,
Regards, Christian