Other Parts Discussed in Thread: CC2540
Hello all,
I'm implementing UART communication between MSP430 and CC2540.
The communication is planned to be using ISR for read and write.
Moreover, I plan to use the CC2540 as mess storage device over USB.
Reading through the "Software Developer’s Guide" I can see under the "Symbols Mandatory for BLE Stack:" section that the definition HAL_UART_ISR is not to be used when planning on using the CC2540 as USB as it is written :
"HAL_UART_ISR – This symbol sets the CC2540/41 UART interface to use ISR mode, and
should be set to TRUE for builds that use the actual UART interface for the HCI, but not for
builds that use the USB (virtual UART) interface."
I was hoping you guys could share some light on how can I accomplish this two tasks.
Thanks in advance!