Hi :
I am designing CC2541and plan to layout few days later. After taking a closer look and do a comparison on the 2.4GHz IFA antenna design on various EVBs, I see some IFA layout not well followed the swra117d. I don't know if that is because of EVB or it is really also ok for end product design. Below are my questions:
1. In CC2541 KeyFob, the antenna ground connected to PCB ground plane on top layer, but in swra117d, it strongly recommend to use a "via" connecting to GND. Both ways are good or only the latter one is recommended for end product design ? Using a "via " is important or just better to follow or doesn't matter ?
Fig 1. Fig 2.
2. In Fig 2 (CC2540 USB ), the antenna gnd follows the swra117d, but why the trace between the antenna gnd and system gnd needs to be a " winding" trace ? can't it be a straight line ? any special reason to design so ?
3. The width of the layout trace of the feeding point / gnd point is also different between fig 1, fig 2 and swra117d , which one is better for me to follow ? use thinner trace width before going to antenna (like Fig 2) or keep the same trace width as antenna (Fig1) ?
Looking forward to your professional advice.
Ray