This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2540 dma configure setting when using in sequence conversion

Other Parts Discussed in Thread: CC2540

Hi,

I want to use four channel ADC of cc2540, input pins are AIN4~AIN5. So set pin4 to pin7 as analogue pins using  APCFG |= 0xF0. But I don't know whether DMA works if I only use one DMA channel for four channel ADC. Can I choose AIN4~AIN5 rather than AIN0~AIN3? I have set DMA as below but it doesn't work. Where is the problem?

Thanks

dma_channel_init ( &dmaConfig0, adc_data, 4, HAL_DMA_TRIG_ADC_CHALL);

 void dma_channel_init ( halDMADesc_t __xdata *dma_p, int16 __xdata *dest_adr, uint8 lenl, uint8 trig )


dma_p->srcAddrH=(uint8)0x70;
dma_p->srcAddrL=(uint8)0xBA;

HAL_DMA_SET_DEST( dma_p, dest_adr );

HAL_DMA_SET_VLEN (dma_p,HAL_DMA_VLEN_USE_LEN);

HAL_DMA_SET_LEN( dma_p, lenl );

HAL_DMA_SET_WORD_SIZE (dma_p, HAL_DMA_WORDSIZE_WORD);

HAL_DMA_SET_TRIG_MODE (dma_p, HAL_DMA_TMODE_SINGLE);

HAL_DMA_SET_TRIG_SRC (dma_p, trig);

HAL_DMA_SET_SRC_INC (dma_p,HAL_DMA_SRCINC_0);

HAL_DMA_SET_DST_INC (dma_p,HAL_DMA_DSTINC_1);

HAL_DMA_SET_IRQ (dma_p,HAL_DMA_IRQMASK_DISABLE);

HAL_DMA_SET_M8 (dma_p,HAL_DMA_M8_USE_8_BITS);

HAL_DMA_SET_PRIORITY (dma_p,HAL_DMA_PRI_HIGH);
}