This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

what is the cheapest way to implement bluetooth 2.x using TI chip solution?

Hi,

 I am interested to know the best and cheapest way to implement bluetooth 2.x using ti chips...

  • Hi Vinod,

    We have the LMX9830, which is a highly integrated Bluetooth 2.0 module.

    It has built-in Bluetooth profiles and allows it to perform Bluetooth communication without a host. The fact that it does not require a controller or processor decreases the system cost significantly.

    We also have the LMX9838, which is similar to the LMX9830, but with even more integration including integrated antenna, EEPROM, crystal, etc.

    They are all fully certified, which also saves certification time and cost.

     

  • Hi, LMX9830 is interesting....

    I bought LMX9838 module. Actually my requirement is high speed data transfer, say I want to send files as fast as possible. What will be the solution for that? The LMX9838 is having a max speed via UART around 931kbps. Is there any way to transfer data at speed around 2.5 or 3mbps ? (any SPI interface)

  • Hi Vinod,

    Apologize for not seeing this post and letting fall through the crack.

    We cannot support up to 2.5 or 3MBPS.

    What is your application?

    Ryan Lin