Other Parts Discussed in Thread: CC2541
Hi,
i am trying to connect Gyroscope (L3GD20) with CC2541 through I2C communication. Im using TI Keyfob Sample program for the same but unfortunately i am not able to establish communication with the device. i have checked the clock pulse in DSO and got the correct clock pulse (33 kHz frequency) and no clock pulses for data were detected on DSO.
My basic problem is that my code was not able to establish I2C communication with the device. I have checked with only I2C start condition but i am not able to receive acknowledgement from the device that means communication link was not established. Checked with all connections and program as well but unfortunately the result is same. can some one please help me to sort out this issue.
Thanks in advance