Hi all,
From the thread I read at: http://e2e.ti.com/support/low_power_rf/f/538/t/108807.aspx
The maximum application throughput data rate is 10.6KB/sec (most optimum value).
If for example, my central is connected to 2 devices, can I say the maximum throughput data rate the central could get from the 2 devices is 10.6KB/sec divide by 2 (assuming each device share the same data load to central)?
And connected to max. 3 devices then 10.6KB/sec divide by 3?
Thank you
Handi