Hi :
I am using CC2541 Keyfob and want to change the reciver gain to high-gain mode so I add one more line of code :: HCI_EXT_SetRxGainCmd( HCI_EXT_RX_GAIN_HIGH ) to the following extracted from keyfobdemo.c
===================================================
switch ( currentTxPowerLevel )
{
case 0:
newTxPowerLevel = -6;
// change power to -6 dBm
HCI_EXT_SetTxPowerCmd( HCI_EXT_TX_POWER_MINUS_6_DBM );
HCI_EXT_SetRxGainCmd( HCI_EXT_RX_GAIN_HIGH );
// Update Tx powerl level in Proximity Reporter (and send notification)
// if enabled)
ProxReporter_SetParameter( PP_TX_POWER_LEVEL, sizeof ( int8 ), &newTxPowerLevel );
break;
=======================================================
There is no problem compliering the code and programming the code into CC2541. However, when I used iphone to test, the BLE connection always fail to link up. The screen of iphone always show "disconnected from peripheral". When I remove the line of the code, then connection can successfully link up again. Can you please advise why I see the problem and how to fix it ?
Thank you very much
-Raymond