This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Define a 128 bit UUID

Other Parts Discussed in Thread: CC2540

Hi, I am defining a uuid like this to use it in advertising data for my CC2540

static const uint8 myService[16] = { 0xD0,  0x00,  0x02C,  0x17,  0x1F,  0x4B,  0x0C,  0xA4, 0x899,  0x8E,  0xCE,  0xB5,  0x31,  0xF4,  0x95,  0x7D };

static uint8 advertData[] = 
{ 
// Flags; this sets the device to use limited discoverable
// mode (advertises for 30 seconds at a time) instead of general
// discoverable mode (advertises indefinitely)
0x02, // length of this data
GAP_ADTYPE_FLAGS,
DEFAULT_DISCOVERABLE_MODE | GAP_ADTYPE_FLAGS_BREDR_NOT_SUPPORTED,


0x11,
GAP_ADTYPE_128BIT_MORE,
myService,
};

But I keep getting this error: 

Error[Pe144]: a value of type "unsigned char const __xdata_rom *" cannot be used to initialize an entity of type "uint8" 

after GAP_ADTYPE_128BIT_MORE for myService