This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PAN1323EMK--where does the BT/BLE/ANT stack reside?

Other Parts Discussed in Thread: MSP430F5438A

Sorry if these seem like rookie questions but I'm looking to order a PAN1323EMK and I'm curious about a couple things:

1)  Does the BT/BLE/ANT stack already reside on the Panasonic part (PAN1323)?  Or, do they need to be installed to the processor with which it is to interface?

2)  Besides the MSP430F5438A  experiment board, it would seem I could use the 5529 Experimenter Board with the PAN1323EMK instead.  Is this true?  (I ask because I already have a 5529 board.)

Thanks in advance

  • Brent Huebert said:

    1)  Does the BT/BLE/ANT stack already reside on the Panasonic part (PAN1323)?  Or, do they need to be installed to the processor with which it is to interface?

    The stack resides on the processor connected to the PAN1323.

    Brent Huebert said:

    2)  Besides the MSP430F5438A  experiment board, it would seem I could use the 5529 Experimenter Board with the PAN1323EMK instead.  Is this true?  (I ask because I already have a 5529 board.)

    The Stonestreet One Bluetopia stack is supported on the platforms indicated in the below wiki site.

    http://processors.wiki.ti.com/index.php/CC256x_MSP430_Bluetopia_Basic_Demo_APPS

    Fortunately, your desired board is among them.

    More information can be found at the following Wireless Connectivity portal.