I wanted to check to see if APTX could be used with the CC2564. Since APTX is a codec I would think this would be possible with an external codec to the CC2564 connected to the CC2564 or the host micro-controller.
Is this possible?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I wanted to check to see if APTX could be used with the CC2564. Since APTX is a codec I would think this would be possible with an external codec to the CC2564 connected to the CC2564 or the host micro-controller.
Is this possible?
Hi Ryan,
It should be possible if your stack (A2DP source/sink) supports it.