Other Parts Discussed in Thread: CC2540, CC2541DK-MINI, BLE-STACK, Z-STACK, CC2530, CC2640, ADS1293, CC2541, TIDA-00096
Hello,
I just installed the latest BLE 1.4 and downloaded the IAR compiler. No choice but to use the latest version which is 8.30.1.
The linker fails when trying to build any of the projects. I notice this has happened before with IAR releases. This seems to be a different error than last time. The evaluation license does not let you download previous compiler releases.
Any ideas?
Linking
Error[e16]: Segment ISTACK (size: 0xc0 align: 0) is too long for segment definition. At least 0xe more bytes needed. The problem occurred while processing the segment placement command
"-Z(IDATA)ISTACK+_IDATA_STACK_SIZE#08-_IDATA_END", where at the moment of placement the available memory ranges were "IDATA:4e-ff"
Reserved ranges relevant to this placement:
IDATA:8-1f VREG
IDATA:21-40 VREG
IDATA:41-42 XSP
IDATA:43-43 DATA_I
IDATA:44-4b DATA_Z
IDATA:4c-4d IDATA_Z
IDATA:4e-ff ISTACK
BIT:0-7 BREG
BIT:80-97 SFR_AN
BIT:a0-af SFR_AN
BIT:b8-c7 SFR_AN
Error while running Linker
Total number of errors: 1
Total number of warnings: 0
Thanks!