This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2541 GAP_DEVICE_DISCOVERY_EVENT status value of 0x13?



Sometimes after a call to GAPCentralRole_StartDiscovery() the status value I receive for GAP_DEVICE_DISCOVERY_EVENT is 0x13.  I haven't found anything in the forums or by searching through the code that gives me a clear understanding of what this means with regard to what went wrong during discovery.

I can say that it only seems to happen when I'm currently in a connection with and receiving heart rate data from a heart rate sensor.  I don't know if other types of peripherals would cause the same behavior as I only communicate with a heart rate sensor currently.  

So basically I have a gapCentralRoleEvent_t.gap.opcode that is 1 (GAP_DEVICE_DISCOVERY_EVENT) and a gapCentralRoleEvent_t.gap.hdr.status that is 0x13 (???)

If I perform 10 consecutive 1 second scans at 5 second intervals while in an active connection with a heart rate sensor half may return fine (status = 0x00), telling me the number of devices that were discovered during the scan, and the other half will return with the status of 0x13 in question.

Any help is greatly appreciated!