Other Parts Discussed in Thread: TUSB3410, BLE-STACK
Hi,
I have installed the RFStudio 7 which includes all necessary drivers as suggested on some of the post but windows recognizes the Cable Connection Devices. I have noticed one thing when adding device manually that there are many options for Texas Instrument 's devices but no device like TI CC45XXXX CDC?
I have Windows 7 64 bit and mini Development kit.
Here is the list for same.
MSP Application UART1
MSP Application UART2
MSP Debug Interface
MSP430 Application UART
MSP-EXP430F5438 USB Serial port
MSP-FET430UIF-CDC
MSP-FET430UIF-VCP
MSP-GANG-CDC
MSP-SA430-CDC
MSP-SA430-SUB1GHZ-CDC
TLC59xxEVM
TUSB3410 Device
TUSB3410 UART EVM
I have noticed one more thing with RFStudio 7 that when I connect the SensorTag on serial port RFStudio detects the CC2541 but unable to detect the usb dongle when connected on CC debugger's serial port.
So anyone please help to resolve the same?
Thanks,
-Sandip