Hello,
I am a University of Delaware Engineering student working on a Senior Design project. I have purchased the CC2541 DK-SENSOR and downloaded the TI app on my iphone to go along with it. I am using the accelerometer sensor in it and currently I can see in the settings the max sample rate is 10Hz, but that is too little for the amount of data I need. I was wondering if there was a way to increase the sampling rate to at least 100Hz or greater and if not, do you have a 3-axis accelerometer with that high of a sampling rate? I appreciate your time in addressing this issue.
Thank you,
Christine Wilkerson