Hi,
I just try to update my sensortag via OTA on iPad. Here are the steps I did:
- I downloaded image 1.5, open it via email.
- activate OTA profile
- select "share files"
- Select "SensortagImgA_v1_5.bin" . I can not select Image B as it always tell me : "wrong image type (...) which is the same as on the peripheral".
- Update start, takes 3 minutes
- A pop-up says "firmware upgrade complete (..) press side button of sensor tag to reconnect"
When I re-enter the apps, it always tell me that my FW version 1.0 . Beside I sometimes get the popup telling that I am using a old firmware.
Any advice to get the firmware updated?
Thanks a lot.
jonathan