Other Parts Discussed in Thread: WL1835MOD, WL1271
We are facing issue in running the sample Bluetooth Demos on WL1835MOD Beagle Cape for Sitara BeagleBone Development Board (White).
We followed below steps:
1) Downloaded “BeagleBoneBluetopiaLinuxProduction_4012_linux_installer2.run” installer from Link: http://www.ti.com/tool/linuxezsdk-am335x-wilink8
2) Installed it on the PC machine and copied it to the board at /opt/ssl1
3) Follow steps from http://processors.wiki.ti.com/index.php/StoneStreet_One_Bluetopia_Platform_Manager_Bluetooth_Stack_for_TI_WL18xx
As below:
root@am335x-evm:/opt/ss1/BluetopiaPM/bin# ./SS1BTPM &
root@am335x-evm:/opt/ss1/BluetopiaPM/bin# ./LinuxDEVM
DEVM>Initialize 1
BTPM_Initialize() Success: 0.
DEVM_RegisterEventCallback() Success: 5.
DEVM>SetDevicePower 1
[ 4865.462097] WL1271: BT Disable
[ 4867.484985] Gpio value is :44
[ 4867.499420] WL1271: BT Enable
DEVM_PowerOnDevice() Failure: -10032, Response Message Timeout.
Function Error.
Note: With the same rootfs and kernel we got WiFi working.
Any comments in case if there is an additional step to be done or ...??
Regards,
Ankur