This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2541 maximum data throughput

Other Parts Discussed in Thread: CC2541, CC2540

Hi experts,

I am using CC2541 and an MCU to send data to tablet. I have some questions.

First, if I have 4 services and connection interval is 10ms, can CC2541 handle the data throughput? one of these service have to send 18byte packet and others send 2-4 byte packet

Second, The MCU send data to CC2541 per 5ms, and I set CC2541 send data to tablet per 10ms (task period: 10ms / conn interval: 10ms). but my tablet show that the CC2541 send data per 5 ms. Where may have problem? Thanks

Third, There should be a minimum value of the connect interval which is 7.5 ms, why can my CC2541 send data per 5 ms?

Thanks for answering the abloe questions.

BR, 

ioootsai