TI has two Bluetooth client devices - keyfob and sensor tag - although similar they have different characteristics. Is there an Android demo application which works with the keyfob. Something which turns ON the simple key press characteristic and receives notifications in some ways similar to but much limited functionality compared to BTool,
There are a number of generic BLE demo apps but these do not set the acceptable keyfob characteristic and then receive notifications from the keyfob (example - key press and accelerometer).
If there is an implementation for Android I would appreciate a pointer to such a demo.