This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

download Version 1.1b of BLE protocol stack

Other Parts Discussed in Thread: CC2540, CC2541

Hi,

We where using the CC2540 for a system that was made somewhere in 2011 (based on the keyfob demo).

Now they have changed the hardware slightly which is ok, but they also changed the cc2540 with the cc2541.

Which is 'pin compatible', but they forget to check if the software needs to be changed.

I didn't make the original SW but I am trying now to convert the software to libary 1.4 but without succes.

It compiles and I can pair with the hardware but only in debug mode, and it doesn't receive or send data. (profile api changed ??)

Is there somewhere were I can download the 1.1B version of the stack, because that is the first time that the 2541 is supported and nearest to the original stack used.

Any help is welcome.

greets,

Marc