This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

iar workbench license

Hi

I have just downloaded a code size limited evaluation version of the iar workbench for cc2540 mini dk. And i could compile the project simpleBLEperipheral with no errors and warnings. I am using ble version 1.4 and iar workbench 8.20. Since this is a code size limited version of 4K, i wonder how i was able to compile.

the .map file has the following info

110 397 bytes of CODE memory
35 bytes of DATA memory (+ 73 absolute )
6 272 bytes of XDATA memory
194 bytes of IDATA memory
8 bits of BIT memory
4 145 bytes of CONST memory

Errors: none
Warnings: none

Can you please clarify?