Other Parts Discussed in Thread: CC2540
I'm trying to compile project of Location sample with C:\Texas Instruments\BLE-CC254x-1.4.0\Projects\ble\SimpleBLEPeripheral\CC2540DB using CC2540F128DK-MINI Keyfob workspace but I get this error:
Error[e16]: Segment ISTACK (size: 0xc0 align: 0) is too long for segment definition. At least 0xe more bytes needed. The problem occurred while processing the segment placement command
"-Z(IDATA)ISTACK+_IDATA_STACK_SIZE#08-_IDATA0_END", where at the moment of placement the available memory ranges were "IDATA:4e-ff"
Reserved ranges relevant to this placement:
IDATA:8-1f VREG
IDATA:21-40 VREG
IDATA:41-42 XSP
IDATA:43-43 DATA_I
IDATA:44-4b DATA_Z
IDATA:4c-4d IDATA_Z
IDATA:4e-ff ISTACK
BIT:0-7 BREG
BIT:80-97 SFR_AN
BIT:a0-af SFR_AN
BIT:b8-c7 SFR_AN
Error while running Linker