This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Call to GAP_LE_Pairability_Mode fails with error code -120

I'm building my own project which is based on the SPPLEDemo_Lite project.  I ran the SPPLEDemo_Lite and this project seems to work fine. 

In my project I'm working with CCSV4.  Note also, I've rebuilt the pertinent libraries following the steps in the pdf titled "Using the Flexible Build Library" so as to include only Server functionality to save space as Client is not needed in my application.

My problem is that when I attempt to set Pairability with the function call GAP_LE_Pairability_Mode I get an error code of -120 which corresponds to BTPS_ERROR_FEATURE_NOT_CURRENTLY_ACTIVE.

Help!

Thanks,

Brent