Other Parts Discussed in Thread: CC2541
Hi,
I'm developing a BLE peripheral device on the CC2541 (using the Keyfob demo project as a base).
I want the peripheral only to be bondable to a single device (i.e. 1 Smartphone) but be able to connect (unpaired) with multiple phones... The idea is to have some characteristics set to GATT_PERMIT_READ (readable by everybody) and some to GATT_PERMIT_ENCRYPT_READ (readable only bye the bonded device), thus only requiring pairing/bonding with the device when reading the encrypted characteristics.
Separating the characteristics permits works great, but now I want the peripheral to disregard new pairing/bonding requests when a previously bond exists... preventing non-bonded devices to read the encrypted characteristics.
To accomplish that I try to set GAP_BONDINGS_MAX = 1 and hope that would do it. However, it is still possible to pair/bond with a second device and read the encrypted characteristic
What have I missed? Do I have to disregard the second pair/bond request manually in the peripheral application?
// Thomas