Hi,
I try to create a new "hidDevSendReport" to use with my remote TI BLE. I use firmware given by TI !
I would like the same that "mouse profile" but with an other ID :
static void hidDevSendReport( uint8 id, uint8 type, uint8 len, uint8 *pData )
--> id : MY_ID
--> type : HID_REPORT_TYPE_INPUT
--> len : 4
--> buf
I can send my data in this function but after I can not send in GATT_NOTIFICATION function.
Function is as follows :
static void hidDevSendReport( uint8 id, uint8 type, uint8 len, uint8 *pData )
{
hidRptMap_t *pRpt;
gattAttribute_t *pAttr;
uint16 retHandle;
// get att handle for report
if ( (pRpt = hidDevRptById(id, type)) != NULL )
{
// if notifications are enabled
if ( (pAttr = GATT_FindHandle(pRpt->cccdHandle, &retHandle)) != NULL )
{
uint16 value;
value = GATTServApp_ReadCharCfg( gapConnHandle, (gattCharCfg_t *) pAttr->pValue );
if ( value & GATT_CLIENT_CFG_NOTIFY )
{
// After service discovery and encryption, the HID Device should request to
// change to the preferred connection parameters that best suit its use case.
if ( updateConnParams )
{
GAPRole_SetParameter( GAPROLE_PARAM_UPDATE_REQ, sizeof( uint8 ), &updateConnParams );
updateConnParams = FALSE;
}
// send notification
lastNoti.handle = pRpt->handle;
lastNoti.len = len;
osal_memcpy(lastNoti.value, pData, len);
GATT_Notification( gapConnHandle, &lastNoti, FALSE );
// start idle timer
hidDevStartIdleTimer();
}
}
}
}
The problem is the value returned by :
value = GATTServApp_ReadCharCfg( gapConnHandle, (gattCharCfg_t *) pAttr->pValue );
The value returned is false so impossible to send my data by BLE.
I already initialized the GattServ with GATTServApp_InitCharCfg function.
Someone has an idea of the problem ?
Thank you very much in advance.
Best regards,
Alex