Hi,
3 Question in my mind.
1) how do i configure the sensor tag to broadcast my custom string.
2) How do i configure the broadcast frequency
3)How do i Configure the broadcast range(e.g. 5 ft)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
3 Question in my mind.
1) how do i configure the sensor tag to broadcast my custom string.
2) How do i configure the broadcast frequency
3)How do i Configure the broadcast range(e.g. 5 ft)
Hi Ankush,
Assuming you are using SimpleBLEBroadcaster as base code:
1. By modifying the variable advertData
2. By modifying the constant DEFAULT_ADVERTISING_INTERVAL
3. In code dynamically by changing the output power with the HCI_EXT_SetTxPowerCmd command. Valid parameters for CC2541 are HCI_EXT_TX_POWER_MINUS_23_DBM, HCI_EXT_TX_POWER_MINUS_6_DBM or HCI_EXT_TX_POWER_0_DBM. If you want really short range, you could also do a poor antenna design... but that's not very efficient.
If you are using the CC254x as a network processsor, you can check out the TI BLE Vendor Specific HCI Guide document that comes with the stack installer.
Best Regards
Joakim