Other Parts Discussed in Thread: WL1835MOD, CC2540, WL1835
Dear Sir,
I am trying to connect WL1835MOD Bluetooth Low Energy(Bluetopia stack on Linux) with CC2540(we call the instrument LBT). The connection is created succesfully but it lasts less that 1 sec.
I connect the WL1835MOD BLE with BLED112 dongle(from Bluegiga, built around CC2540) with no problem.
If I try Dongle-LBT connection, there is no problem too.3286.ProblemConnect.rar
Following you can see the command and responses of the first scenario process and attached are the FTS logs of WL1835+ bluetopia enabled stack debugging
GATM>ConnectWithRemoteDevice 1CBA8C1B7635 1
Attempting to Connect With (LE) Remote Device: 1CBA8C1B7635 (Flags = 0x80000000).
Local Device Properties Changed.
Device Flags: 0x80000000
LE Scan Mode: FALSE, 0x00000000
LE Adv Mode: FALSE, 0x00000000
LE Slv Mode: Not in Slave Mode
GATM>
LE Device Discovery Stopped.
GATM>DEVM_ConnectWithRemoteDevice() Success: 0.
GATM>
GATT Connection
Connection Type: LE
Remote Address: 1CBA8C1B7635
MTU: 23
GATM>
Remote Device Connection Status: 1CBA8C1B7635, 0 (SUCCESS)
GATM>
Remote Device Properties Changed.
BD_ADDR: 1CBA8C1B7635
Address Type: Public
LE Type: Dual Mode
Device Flags: 0xC00C8001
LE Connect State: TRUE
GATM>
GATT Disconnect
Connection Type: LE
Remote Address: 1CBA8C1B7635
GATM>
Remote Device Properties Changed.
BD_ADDR: 1CBA8C1B7635
Address Type: Public
LE Type: Dual Mode
Device Flags: 0xC0080001
LE Connect State: FALSE