This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540 USB Evalution Kit in Ubuntu 12.04 (Linux) Installation

Other Parts Discussed in Thread: CC2540

Hello,

I am getting issue in installation of CC2540 USB EK module in Ubuntu 12.04 64 bit version as well as in our board having linux kernel version 3.8.0 with bnep enabled.

When I plug in the device into USB port of the PC then it is detected as a high speed USB device but it is supposed to be detected as bluetooth dongle.
sanjay@sanjay-ubuntu-12:~$ dmesg
[70362.504354] usb 1-3.3: new full-speed USB device number 25 using ehci_hcd
sanjay@sanjay-ubuntu-12:~$ lsusb
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 002 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
Bus 003 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
Bus 004 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
Bus 005 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
Bus 001 Device 021: ID 05e3:0608 Genesys Logic, Inc. USB-2.0 4-Port HUB
Bus 002 Device 002: ID 413c:2106 Dell Computer Corp. Dell QuietKey Keyboard
Bus 002 Device 003: ID 046d:c05a Logitech, Inc. Optical Mouse M90
Bus 001 Device 025: ID 0451:16b3 Texas Instruments, Inc.
Bus 005 Device 004: ID 10c4:ea60 Cygnal Integrated Products, Inc. CP210x Composite Device
Bus 001 Device 023: ID 14cd:125a Super Top
After detection /dev/ttyACM* interface must be created. But it is not creating the interface.
sanjay@sanjay-ubuntu-12:~$ ls /dev/ttyACM*
ls: cannot access /dev/ttyACM*: No such file or directory

I tried with installing python-serial packages as per instructions but unable to find the proper solution.
I am following below mentioned links:
https://github.com/Harper04/Python-for-TI-CC2540
http://processors.wiki.ti.com/index.php/Category:LinuxHostTest2

Please help me to come out of this.

Thanks and Regards
Sanjay K Dwivedi