I have the ethermind bluetooth stack running on the MSP430FBT5190 in conjunction with the PAN1325A.
The code works on the MSP-EXP439F5438 experimenter board and you can see the device via
bluetooth when performing a search (which uses the PAN1315ETU but that shouldn't make a difference).
This same schematic has been transferred to our own development boards. However when you run the firmware
the bluetooth device is not visible. I have scoped the data on the TX,RX, slow clocks lines and it looks good
(voltages are the correct levels & frequencies (baud rate = 115200) look good)
The PCB layout has been performed in accordance with the recommended design guidelines (no copper ground
plane, vias under the pads, edge of the board, etc.) . The production was performed by a contractor but they
were instructed to follow the reflow temperature requirements stipulated in the datasheet.
Has anyone else experienced this problem ?