This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSR Tiwi-ub1 connection to CC debugger issue [Resolved]

Hi,

I would like to connect very simply my LSR (LS Research) BLE module to TI CC debugger and it does not work.

Is anyone around has used this module ?

Here is my connection:

DEBUGGER    Module

VCC                    pin 11,12

GND                   pin 22

DBG_CLK         pin 7

DBG_DATA        pin 8

nReset               pin 6 through 2K7 resistor 

I also added the external 32K crystal (same ref as the TI Keyfob demonstration board) on the pins 4/5 with its 12pF capacitors.

Impossible to have a green light on the CC DEBUGGER even after applying reset on it... What do I have to do ? Thanks a lot for your support... help...