Hi
I have an application using CC2541 and the Ti 1.4.0 stack running as a peripheral, where the peak current I can draw from the battery is very limited, and so is the room for decoupling capacitance. Therefore I need to make sure that the CC2541 is not using the radio at some short and rare time-instances where another component needs to use the battery alone.
Is it possible to control when the stack will skip connection events, or otherwise force a short radio "silence" without dropping the connection?
Best Regards,
Morten