Hi ,
we are working for sensor product using CC2541.
It has multiple sensors such as Temp,pressure,humidity,ALS & other Gas sensors using ti AFE.
Also we are planning to add GPS module to CC2541 through UART.
Does the internal flash & RAM size of CC2541 supports all the above sensors and GPS service?
Also we need to store the measured data over 24hr period.
or we need to used CC2541 as network processor by connecting to external host.
please give me the approximate foot print size for the above application.