This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX9838 send data but no reply

Other Parts Discussed in Thread: ASH

Hello Fellow Engineers :-)

I'm working on a project using the LMX9838 Bluetooth Serial Port module.

So far I have had no problem at all with this module. It works very well.

Now I have stumpled upon a mysterious issue.

When transmitting data using the command interface and command SPP_SEND_DATA, I should be able to transmit a total payload of 330 bytes cf. the software users guide. If I transmit 330 bytes + the command interface around the data, the module simply does not respond. If I transmit e.g. 200 bytes, there's no problem at all. I have found the limit to be 252 bytes.

Best Regards