Hello all,
I know the CC2540/1 is only capable of sending more than 4 packets if you use overlapped processing, but if I remember correctly, the improvement was to only 4-5 packets.
I am now running another chip (CSR) which is sending 16 packets per connection event, within a connection interval of 12.5 ms. The CC2540 sniffer is able to sniffer all these packets
Interestingly, if I reduce the connection interval to 7.5ms, the sniffer no longer can pick up the packets
So, my questions are, is this behaviour expected. While the CC2450 can only send 4 packets per connection event, can it read alot more?
Image:
http://gyazo.com/d0c7c3b85ea4bca477826760f42d3010
Thanks
Thomas