This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2541 Software UART

Other Parts Discussed in Thread: CC2541, MAX232

Hello All,

I need to know, is there anyway I can use the software UART for P1_0 pin and P1_1.Because i have this pin option only.

Can anybody support me for this.Code for just transmitting is enough.

Also will Max232 works for converting CC2541 output to UART.

  • Hi Selva,

    yes, of course you can implement software UART using those pins, I can't see why not. However I can't find any examples for the CC2541. You can try to google for "UART bit bang".

    Anyway MAX232 is a UART-RS232 converter device, so it is a level/voltage shifter only.