Hello,
I am a student working on a Break Disc Project. Therefore i would like to use the cc2541's bluetooth, i2c,... functions.
I've got a simple question:
As the cc2541 has a 8051 Core, it should be able to use the Ulink2, because it is supported. But the cc2541 is not on the list of the supported devices of the ulink2.
Can someone tell me the reason why that is? I would apprechiate that! Thank you a lot.
Matthias