Dear CC256x community,
I have a question regarding production line testing of the CC2564 in low-energy continuous TX mode. My problem is that my Anritsu Bluetooth tester always reports "Not enough measurements" for any TX tests. All RX test work, but not the TX tests.
I believe that my CC2564 is configured correctly, service pack is loaded, all HCI commands I observe are replied to correctly by the chip. I also configured the test mode parameters using HCI_VS_Set_LE_Test_Mode_Parameters (0xFD74) as indicated on TI's webpage http://processors.wiki.ti.com/index.php/CC256x_Testing_Guide.
Usually, the last thing the Bluetooth tester does before starting a TX test is issue the HCI command HCI_BLE_Transmitter_Test (0x201e), which gets a correct reply from the CC2564. However, after this, nothing happens. The Bluetooth tester does not show any TX traffic on the configured channel.
I can confirm that in normal use the CC2564 works just fine in our application. I am only having trouble with the TX tests in production line testing.
Did anyone face the same problem? Any ideas from a TI expert?
Thanks and best regards,
Severin Leven