This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bonding without passkey

Other Parts Discussed in Thread: CC2540

I don't want to input passkey on bonding between iPhone(Central) and CC2540(peripheral). Is it possible to bypass to input passkey?
  • Yes, that is the 'just works' pairing scenario.  

    uint8 mitm = FALSE;
    uint8 ioCap = GAPBOND_IO_CAP_NO_INPUT_NO_OUTPUT;

    GAPBondMgr_SetParameter( GAPBOND_MITM_PROTECTION, sizeof ( uint8 ), &mitm );
    GAPBondMgr_SetParameter( GAPBOND_IO_CAPABILITIES, sizeof ( uint8 ), &ioCap );

  •     Thank you very much. It works well with following code.

        uint32 passkey = 0; // passkey "000000"
        uint8 pairMode = GAPBOND_PAIRING_MODE_WAIT_FOR_REQ;
        uint8 mitm = FALSE;
        uint8 ioCap = GAPBOND_IO_CAP_NO_INPUT_NO_OUTPUT;
        uint8 bonding = TRUE;
        GAPBondMgr_SetParameter( GAPBOND_DEFAULT_PASSCODE, sizeof ( uint32 ), &passkey );
        GAPBondMgr_SetParameter( GAPBOND_PAIRING_MODE, sizeof ( uint8 ), &pairMode );
        GAPBondMgr_SetParameter( GAPBOND_MITM_PROTECTION, sizeof ( uint8 ), &mitm );
        GAPBondMgr_SetParameter( GAPBOND_IO_CAPABILITIES, sizeof ( uint8 ), &ioCap );
        GAPBondMgr_SetParameter( GAPBOND_BONDING_ENABLED, sizeof ( uint8 ), &bonding );