Hi TI Community:
I am unable to get a response from a CC2540. I would appreciate any assistance. Thanks, in advance.
I am building a new home entertainment system called Votsh Waves (Details at http://www.votsh.com). I have constructed a custom pc board that has an Atmel ATmega256RFR2 and CC2540. The CC2540 has the HostTestAPP installed. The pin connections are:
2540 ATmega256RFR2
37 P1_7 TX1 <--> PD3
38 P1_6 RX1 <--> PD2
I wrote a sketch in Arduino IDE as:
#include <Arduino.h> // Arduino main libraries
#include <SPI.h> // Serial Device Interface
#include <Wire.h> // TWI/I2C library for Wiring & Arduino
unsigned long time = 0;
int firsttime = 1;
void setup(){
Serial1.begin( 115200 );
Serial.begin( 115200 );
time = millis();
}
void loop(){
while ( Serial1.available() )
{
Serial.print( "Received " );
byte data0 = Serial1.read();
Serial.print( data0 );
Serial.println( "." );
}
if ( firsttime )
{
firsttime = 0;
Serial.println( "BLE Experiment Started" );
}
// Do this every 1 second
if ( ( time + 2000 ) < millis() )
{
time = millis();
Serial.println("Sending command");
byte buf[] = { 0x01, 0x09, 0x10, 0x00 };
Serial1.write(buf, 4);
}
}
I chose the commands (x01, x09, x10, x00) from notes I found at http://e2e.ti.com/support/wireless_connectivity/f/538/t/206742.aspx. These command bytes should return the board address, according to the forum page.
I download the sketch to the Arduino, open the Serial Monitor and see:
BLE Experiment Started
Sending command
Sending command
Sending command
Sending command
There is no response from the 2540.
Any assistance would be greatly appreciated. Thank you.
-Frank