This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to increase Master BLE data rate

Hello Everyone,

We are current using a BLE Master to transmit a file to slave of approx. 400 KB, it takes about 7 mins to transfer this file.

Our objective is to reduce this time,

We used a sniffer to analyze this slow data rate and we found out that there only 20 bytes are transferred in a single packet

In the transmit window. Please suggest how to increase the data rate, our configuration is as follows:

Connection interval : 7.5ms

Slave Latency : 0

Supervisory timeout: 90 ms

 

We are in completion phase of our development, please suggest us a solution to increase the upload speed.

 Regards

Sangram