This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Serial Bootloader timeout when verifying



Following "BLE Developer’s Guide for  Over-the-Air Download for CC254x  Version 1.2".

It works fine up to the actual OAD. The bin-file transfer using Serial Bootloader Demo Tool (V1.2) from PC to the SmartRF05 board is unable to complete. Data packets are sent OK but when the verifying phase starts, it's seems unstable and eventually ends up in a "Timeout waiting for response from target"-message. The verified packets count before timeout varies.

Using a USB-to-serial port (COM26) with hardware handshake and a full RS-232 serial cable.

Anyone seen this before? Anyone got a solution?