Hi all,
for long time I am using packet sniffer with cc2540 USB dongle
but most of the times whenever I try to connect to slave device from master
my packet sniffer gets hang and it occurs most of the time.
I think the issue is with cc2540 dongle firmware which fails most of the time
when most of the packets being exchanged between master and slave
and during connection establishment between the two
TI kindly suggest solution for the same
Regards,
sarang