This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Module support for CC2564B

Other Parts Discussed in Thread: CC2564MODN, MSP430F5438A

Hi,

Please go through my understandings and problems I face below and provide clarifications:

1) I chose CC2564B to implement dual mode bluetooth functionality in my product. '2564B' particularly because it is a dual mode chip and supports assisted A2DP profile. I need audio sourcing in my product and hence A2DP profile is mandatory.

2) The module available with integrated CC2564B is PAN1326B from Panasonic.

3)  For developing a prototype for my product, I need an evaluation board containing PAN1326B module because only PAN1326B contain CC2564B which support A2DP profile.

               Qn1: Which evaluation board can I choose?

               Note: I found PAN1323-ETU which doesnt contain CC2654B.

4) I should interface an MCU with PAN1326B in my product, and hence for prototyping I require another evaluation board which  contain that MCU. MSP-EXP430F5438 experimenter board containing MSP430F5438A seems OK for me.

              Qn2: Is SDK support with assisted A2DP profile available for MSP430F5438A  MCU?