This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Android 4.3 connect HID mouse FAIL

Hi Ti,

I get a fatal issue,connect to HID mouse fail

 When mouse idle device will auto disconnection.  

Please check as below log

Thanks

Ben

I/power   (  883): release_wake_lock id='brcm_btld'
E/bt-btm  (  883): btm_sec_disconnected - Clearing Pending flag
W/bt-btif (  883): bta_hh_co_close: dev_handle = 0, app_id = 1
W/bt-btif (  883): bta_hh_co_close: Found an existing device with the same handle dev_status = 0, dev_handle =0
W/bt-btif (  883): bta_dm_act no entry for connected service cbs
I/power   (  437): acquire_wake_lock lock=1 id='KeyEvents'
I/power   (  437): release_wake_lock id='KeyEvents'
D/HidService(  883): Connection state 00:1F:20:15:B1:AD: 2->0
I/power   (  437): acquire_wake_lock lock=1 id='KeyEvents'
I/EventHub(  437): Removing device '/dev/input/mouse0' due to inotify event
I/power   (  437): release_wake_lock id='KeyEvents'
D/BluetoothAdapterProperties(  883): CONNECTION_STATE_CHANGE: 00:1F:20:15:B1:AD: 2 -> 0
D/BluetoothAdapterService(1104993568)(  883): Get Bonded Devices being called
D/BluetoothAdapterProperties(  883): getBondedDevices: length=1
I/power   (  437): acquire_wake_lock lock=1 id='KeyEvents'
I/EventHub(  437): Removing device '/dev/input/event7' due to inotify event
I/EventHub(  437): Removed device: path=/dev/input/event7 name=Broadcom Bluetooth HID id=8 fd=209 classes=0x80000169
I/InputReader(  437): Device removed: id=8, name='Broadcom Bluetooth HID', sources=0x01002713
V/InputManager(  437): Eddie: updateUsbCamera
D/CachedBluetoothDevice(  737): onProfileStateChanged: profile HID newProfileState 0
D/dalvikvm(  737): GC_CONCURRENT freed 421K, 5% free 10062K/10580K, paused 3ms+7ms, total 38ms
D/DOMX    (  127): hardware/ti/domx/domx/omx_proxy_common/src/omx_proxy_common.c:1406   __PROXY_SetParameter()
D/DOMX    (  127): ERROR: failed check:(eError == OMX_ErrorNone) || (eError == OMX_ErrorNoMore) - returning error: 0x80001001 - Error returned from OMX API in ducati
D/DOMX    (  127): hardware/ti/domx/omx_proxy_component/omx_camera/src/omx_proxy_camera.c:476   CameraSetParam()
D/DOMX    (  127): ERROR:  CameraSetParam: Error in SetParam 0x80001001
E/CameraHal(  127): (b7b3a9b8)   hardware/ti/omap4xxx/camera/OMXCameraAdapter/OMXCameraAdapter.cpp:4316 fetchCapabiltiesForMode - Error while configuring camera mode in CameraAdapter_Capabilities 0x80001001
E/CameraHal(  127): (b7b3a9b8)   hardware/ti/omap4xxx/camera/BaseCameraAdapter.cpp:2721 CameraAdapter_Capabilities - supportedCameras= 0
E/CameraHal(  127): (b7b3a9b8)   hardware/ti/omap4xxx/camera/CameraProperties.cpp:117 loadProperties - camera busy. properties not loaded. num_cameras = 0
E/CameraHal(  127): (b7b3a9b8)   hardware/ti/omap4xxx/camera/CameraHal_Module.cpp:776 camera_get_number_of_cameras - Unable to create or initialize CameraProperties
I/power   (  437): release_wake_lock id='KeyEvents'
I/ActivityManager(  437): Config changes=1460 {1.0 ?mcc?mnc en_US ldltr sw360dp w360dp h615dp 320dpi nrml long port finger -keyb/v/h -nav/h s.7}
I/power   (  437): acquire_wake_lock lock=1 id='PowerManagerService.WakeLocks'
D/LocalBluetoothManager(  737): setting foreground activity to null
D/PhoneStatusBar(  630): mSettingsPanelGravity = 55
D/dalvikvm(  737): GC_FOR_ALLOC freed 102K, 6% free 10001K/10604K, paused 24ms, total 24ms
I/dalvikvm-heap(  737): Grow heap (frag case) to 9.819MB for 23312-byte allocation
D/dalvikvm(  737): GC_FOR_ALLOC freed 5K, 6% free 10018K/10628K, paused 20ms, total 20ms
D/dalvikvm(  737): GC_FOR_ALLOC freed 3K, 6% free 10039K/10628K, paused 20ms, total 20ms
I/dalvikvm-heap(  737): Grow heap (frag case) to 9.870MB for 36880-byte allocation
D/dalvikvm(  737): GC_FOR_ALLOC freed <1K, 6% free 10075K/10668K, paused 19ms, total 19ms
D/LocalBluetoothManager(  737): setting foreground activity to non-null context
D/BluetoothDiscoverableEnabler(  737): handleModeChanged(): mode = 23
D/BluetoothDiscoverableEnabler(  737): handleModeChanged(): mode = 23