Dear TI,
I have a question about the power consumptions for starting up CC2541.
I'm using the CC2541 with the sample project "SimpleBLEPeripheral" in BLE-CC254x-1.4.0 (IAR EW).
and I have a problem that the power comsumption is huge for starting up.
I used an ideal voltage source to provide a 3V voltage for monitoring the start-up operation,
and I found that the start-up mode lasts for about 500ms with a steady current of about 8mA.
This power consuption is really huge for BLE, in my opionion.
Is there anyway to reduce the current in the start-up mode or anyway to reduce the start-up time?
Best regards,
HG